Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST10 Maintenance Packs

Phenom
Phenom

I believe the MPs are cumulative. So MP2 will include MP1 and MP2. Likewise, MP3 will include MP1,2 and 3. Does that help?

Re: ST10 Maintenance Packs

Phenom
Phenom

@RyanM

Yes, I was aware of that.

My question was more of what am I left with if I uninstall a MP.

I think ukdave makes it clear that it will revert back to the last installed MP - so if you have only installed that one (as we will do) you would step back to base install, and would then have to install MP1 or 2.

If you want the ability to step back one MP at a atime then you need to install each sequentially.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.