Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 - Sheet metal - Corner

Phenom
Phenom

I try to clean a corner on my sheet metal part, but can't see how to do this correct:

OmcLMAr

Any suggestions?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
10 REPLIES 10

Re: ST10 - Sheet metal - Corner

Valued Contributor
Valued Contributor

Hi~

youtube Video :

 

URL : https://youtu.be/Se337uy7MHo

 

 

Re: ST10 - Sheet metal - Corner

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Joris,

 

A couple of options.....one, you could adjust the side angle of the flange to 45 degrees, and that would get it close.

 

Capture [20171026-2152].PNG

 

Two, you could change the process a little, making a rectangular tab first, then just extend the contour flange to those two edges, and the mitered corner is made automagically.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST10 - Sheet metal - Corner

Valued Contributor
Valued Contributor

solid Works Multi flange video...

URL : https://youtu.be/boMQGqgCNR0?t=239

 

 

Doing this on solid Edge is cumbersome.
See a video of solid works.

This is the feature I want to apply to the edge.

Betreff: ST10 - Sheet metal - Corner

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

 

 

easiset way here is to use a different approach right from the beginning.

 

Do not start with a contour flange, a cut out and two flanges.

 

Just start with a flat tap and a single contour flange.

 

That's it!

 

 

regards
Wolfgang

Betreff: ST10 - Sheet metal - Corner

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

 

 

another also very easy way would be to do as suggested by @Hclee to use the angle value for the flanges and set them to 45 degrees

 

regards
Wolfgang

Betreff: ST10 - Sheet metal - Corner

Phenom
Phenom

Thanks all!

I'll test it this afternoon.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Betreff: ST10 - Sheet metal - Corner

Valued Contributor
Valued Contributor

Hi hawcad..

I do not care about this question, but I would like to ask you.
I saw your macro DFTtoDXF Macro ..
It was using a separate option file ini.
It is very exciting for me.
If not, can I see the code that used the ini file?
I would also like some code.

Re: ST10 - Sheet metal - Corner

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Just an other solution:

 

BR,

Imi

Imics
http://solidedgest.wordpress.com/
Highlighted

Betreff: ST10 - Sheet metal - Corner

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

this is nothing secret nor special.

 

I simply have used those old vb6 INI procedures.

If You google for read from INI You will get tons of code and examples.

 

But to be honest.

 

I have changed my codes a while ago to use XML instead of INI.

This has to do with 2 reasons:

  1. XML read/write parser syntax is easier and better to use, I think more flexibel too 
    and
  2. I have seen that with this old INI code I had problems under Win10
    I have seen cases where the read from INI file delivered wrong results even if the code was exactly the same, the ini file was the old one but it didn't worked right.

 

 

 

regards
Wolfgang