Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 - dimension to rounded edges will not be retrieved

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,



as mentioned in another post regarding virtual edges, I have seen, that dimension to such virtual edges are not be retrieved from 3D to draft,

 

Same dim to a sharp edge is retrieved to draft.

 

 

Is this the same in ST9 (just updated all computers here to ST10) or is this a bug from ST10?

 

20170810_2239.PNGpart20170810_2240.PNGdraft

regards
Wolfgang
9 REPLIES

Re: ST10 - dimension to rounded edges will not be retrieved

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @hawcad,

 

Probably a failing on my part, but I have never used the retrieve dimension functionality, well, in production anyway.....so can not say if this is how it was in ST9....we're on ST10 now also.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST10 - dimension to rounded edges will not be retrieved

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SeanCresswell

 

 

 

thanks for answering.

 

 

I have used the Dimension Retrieving very often (it really makes sense) but to be honest, in most cases the dims are orthogonal and this will work with ST10 too 

regards
Wolfgang

Re: ST10 - dimension to rounded edges will not be retrieved

Good morning Wolfgang,

 

I did a quick test in ST9 and see the same behaviour. ST9 is not retrieving dimensions of virtual edges.

 

Regards,

Theodore

 

Capture.JPGCapture_A.JPG

 

 

Kind regards,
Theodore Turner

Solid Edge 2019 MP4
Teamcenter 11.3

Re: ST10 - dimension to rounded edges will not be retrieved

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @TheodoreTurner

 

 

 

thanks a lot for testing and answering.

 

I never realizd that thos dimension are not retrieved.

Maybe this always was exactly so, or came in with ST8,9

 

Anyway, it is like it is!

 

Thanks for helping

 

regards
Wolfgang

Re: ST10 - dimension to rounded edges will not be retrieved

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Not working even in ST8 @hawcad if it helps to fully confirm !

Re: ST10 - dimension to rounded edges will not be retrieved

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

thanks, so this seems to become a more and more.

"Oh, I thougt it always was just so!"

 

but obviously not

 

regards
Wolfgang

Re: ST10 - dimension to rounded edges will not be retrieved

Community Manager Community Manager
Community Manager

Slightly OT, but did you know in ST10 that retrieved PMI are fully associative? This means you can really put the intelligence in the model if you like -- if you put in tolerance in the model and treat it as the master and later change the tolerance, the dimension in the draft will update. This is pretty nice for those of you trying to get to more of an MBD (Model Based Definition) approach to things, where all the intelligence is in the model.

Dan Staples
Director, Solid Edge Product Development

Re: ST10 - dimension to rounded edges will not be retrieved

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @dcstaples

 

 

 

Yes, have seen it in the What's New, and after waiting for years this was one of my happiest moments in my SE life!

 

 But to be honest, this also was one of those things I never ever understood, that a change in tolerances will not be reflected in the draft update.

There even was no info sign or message to show, that this happend.

 

So drafts run out of actuality without given any notice to the user.

Sorry to say it like this: I see this not as much as an improvement but more as an error fix!

 

 

regards
Wolfgang

Re: ST10 - dimension to rounded edges will not be retrieved

Phenom
Phenom

How about an update for intersections to be driving?  many times I'll draw extension lines just so I can dimension to them.

-Craig