Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 drops Viewer but what about insight?

Valued Contributor
Valued Contributor

Correct me if i am wrong. ST10 does not have the viewer now but uses a watered down solid edge to view files. I have been told this new viewer will not work with viewing files that are still in insight? is this correct?

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

10 REPLIES 10

Betreff: ST10 drops Viewer but what about insight?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ngardner

 

 

so in this case (if it true) I would install "View & Markup" which can be downloaded extra from download server full products.

 

See post regarding old macros where this also solves a serious of problems.

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Error-when-firing-up-an-quot-old-qu...

 

After installing View & Markup You will have available the old Insight Connetc Viewer and the old free Solid Edge Viewer

 

regards
Wolfgang

Re: ST10 drops Viewer but what about insight?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't know about Insight, but the new viewer is the same Solid Edge ST10 application, not a watered down application.  It is rendered a viewer by turning off menus and functions if there is no valid license for anything else (delete the license in the "Preferences" folder and when the License Wizard appears, pick the option "I want to use the Viewer Mode/Free 2D Drafting").

 

On another note, View & Markup is still delivered with ST10 but is not installed as part of ST10.  It is a separate install.  



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST10 drops Viewer but what about insight?

Phenom
Phenom

We are currently on ST7 but are testing ST10.

Would using ST10 as viewer only 'upgrade' earlier version files to ST10 ?

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: ST10 drops Viewer but what about insight?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @beachcomber

 

 

I would like to say "NO" since You will not be able to save anything.

And as long as I can't save anything I also can't change or update anything.

 

 

regards
Wolfgang

Re: ST10 drops Viewer but what about insight?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Only if you saved.  I believe the Draft is all you can save when it is in Viewer/Free2D mode.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST10 drops Viewer but what about insight?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

Hi @ngardner

 

 

but I think a draft also only can be saved as long as there is no 3D data in use.

Otherwise it would be possible to finish a draft which comes from a 3D part/ASM

 

 

regards
Wolfgang

Re: ST10 drops Viewer but what about insight?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @KennyG

 

 

 

OK, You are right, You can save a draft with the 2D license, even when it shows a 3D part.

You will not be able to add any dimensions etc. but You are able to save it and therefore to bring the last saved version up to ST10

 

So @beachcomber this means You have to be carefull when installing the ST10 with 2D license as viewer.

 

regards
Wolfgang

Re: ST10 drops Viewer but what about insight?

Phenom
Phenom

Thanks all.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: ST10 drops Viewer but what about insight?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I was discussing this with a customer last week nad we learned that you can move an delete dimensions on a view derived from a 3D model then save. This was concerning to them.

 

It looks like you can set the default to open as read only but the user is still able to change that of they wanted.

I was hoping the SEAdmin would allow me to force readonly but I didn't see it.

If anyone knows of a way to lock down SE to behave as a viewer only I would be interested.

LMGi
www.TLMGi.com