Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST10 is out

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@LauraWatson  "Solid Edge ST10 is the first multilingual release.  All 14 languages will release at the same time."

 

That statement is AWESOME!



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST10 is out

Valued Contributor
Valued Contributor

I've always updated SE as soon as the CD/DVD arrives on my desk.

Never had any problems, and I've been doing it this way since SE V7!

 

Can't wait for ST10

Matt Hunt IEng.MIED
Design Engineer
M-Flow Technologies

ST10 MP*
K2200

Re: ST10 is Announced (not avaialble till mid to late summer)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just updating the subject line.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST10 is out

Phenom
Phenom

I can't wait neither.

But I have had issues. For example the connect cone-cone was lost once.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: ST10 is out

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,


I thought that I have read something about that ST10 will NOT be able to run under Win 7 and will need atleast Win 8 or better 10.

 

Can anybody confirm that or is this only something in my mind?

 

regards
Wolfgang

Re: ST10 is out

Valued Contributor
Valued Contributor

Hellow hawcad..

I knew so too.
There are many users of Win7 than win10
I think it is longer.

Highlighted

Re: ST10 is out

Phenom
Phenom

From the ST9 release notes:

 

• Solid Edge ST9 is 64-bit only. Solid Edge ST6 was the last release of 32-bit Solid Edge.
• Windows 8 Home, Windows 10 Home, and Windows RT are not supported.
• Solid Edge stops certifying new releases against an operating system shortly after
Microsoft drops mainstream support for it. Solid Edge ST9 will not install on Windows
Vista or Windows XP. Microsoft dropped mainstream support for Windows 7 in January
2015. Solid Edge ST9 continues to install on Windows 7, however, if there is a Windows
7 specific problem, we cannot guarantee that a fix can be provided if support is required
from Microsoft.
• Solid Edge ST10 will be the last release to support Windows 7.
• Solid Edge does not support the new Windows 10 browser, Microsoft Edge.

Re: ST10 is out

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alex_H

 

 

 

thanks for clarify and finding the text

 

So it seems as ST10 will be possible with win7 too.

 

 

regards
Wolfgang

Re: ST10 is out

Pioneer
Pioneer

What are the system requirements for ST10?

Re: ST10 is out

Legend
Legend

Just a side question.
With ST9 online help still going to Internet Explorer, will this be updated / changed in ST10?
Would be nice if the online help function would use the default internet brwoser from now one.

--------------------------------------------------
Marc Boom
marc.boom@outlook.com