Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST10 issue with assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does anyone know a good way to prevent msft from pushing the update? What settings need to be adjusted?

I selected the option to defer or delay feature updates but it says it only works for about a month.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST10 issue with assemblies

Phenom
Phenom

@bshand To answer your question, how to defer updates, it depends on the version of Windows 10 you are running. Here is a pretty good article that covers the basics. But you have to remember that upgrades are different from security patches and Home is different from Pro.

I'm running Pro and have more options than my daughters laptop running Home.

 

For the Pro user you can set the update to the Semi-Annual Channel which means it has more testing.

Feature updates can be set for updates to occur any day during a full year (1-365).

Security updates can be set for a month delay (1-30).

Highlighted

Re: ST10 issue with assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RyanM, The article talks about the setting I mentioned. But it has some different verbage and mine says updates are only paused until 2/9/2018.

deferupdates.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200