Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 questions

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Edgers,

 

Can there be problems opening files with ST10 that have not been opened since the first versions of Solid Edge?

Would it be convenient to use the OpenSave utility?

 

 

Best regards,

Xènia,

2 REPLIES 2

Re: ST10 questions

Legend
Legend
A few months ago I opened a project done in V7 and there were no problems, very impressive....

Around version 4 Solid Edge changed kernel to the parasolid Kernel... no idea if the files done in this era can be loaded ?

Kind Regards,


Jan Bos

Re: ST10 questions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have v4 or earlier model files, they will not open in current versions.  Going from memory a long time ago, but I believe V5 was the only version that would update them from the ACIS kernel to the PARASOLID kernel.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com