Cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 sheetmetal cutout bug?

Gears Phenom Gears Phenom
Gears Phenom

ST10, ordered sheetmetal, "normal cutout"  after creating the profile and closing sketch, by default I get the warning triangle "part not modified edit the feature inputs".  To correct this this I simply need to select the extent of the cut, thru all, thru next, surface selection, etc..   Even though the "thru next" is highlighted I alwasy have to re-click the button for it to work. Previously a directional arrow would pop up automatically to select direction of cut.

Same goes for "slot" & "cut" command.

Just me?

-Craig
4 REPLIES 4

Re: ST10 sheetmetal cutout bug?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Working normally for me.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST10 sheetmetal cutout bug?

Honored Contributor
Honored Contributor

I remember reading that "normal cuts" in sheet metal were going to be updated, but I have not looked at ST10 yet. I hope we can cut through close corners now with angles other than 90 deg to the bend.

Re: ST10 sheetmetal cutout bug?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Craig_H,  working "normal" here also.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST10 sheetmetal cutout bug?

Gears Phenom Gears Phenom
Gears Phenom

Weird.. I'l keep trying to see what makes a change.

-Craig