Cancel
Showing results for 
Search instead for 
Did you mean: 

ST4, Large assembly management

Genius
Genius

We  have lot of assemblies Creo and Solid edge. In  Creo(ProE), We are able to create simplified representation management different configration. Do we have any similar option in Solid edge ST4?

 

Regards

Venny

2 REPLIES 2

Re: ST4, Large assembly management

Genius
Genius

Solid Edge has two modes of simplification:

 

1. At the part level (.par & .psm), parts can be defeatured to reduce the overhead in a large assembly. This is effectively a simplified configuration. After the part has been "simplified", the part or an assembly in which the part resides can be opened using either the designed or simplified configuration.

 

2. At the assembly level it is also possible to create simlifications. In my experience this works best with enclosures that contain lots of internal parts that you are not concerned with at a higher level. In the assembly simplification it creates more or less a shrinkwrap around the outside of the enclosure and displays it without the contents.

 

I don't use either simplification much, even though our assembly model is large, but they are available. Others may be able to speak to specifics of usage. Check Help for simplify in parts and assemblies.

Bob Henry

Manager of Engineering - Highwall Miners
Caterpillar Global Mining LLC
Houston, PA

Re: ST4, Large assembly management

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

A reference video to Bob's Point (2):