Cancel
Showing results for 
Search instead for 
Did you mean: 

ST4 running slowly

Not applicable
Hi Guys
Just recently ST4 has started taking extra time to complete drawing lines etc, and i have to wait for the focus to return to the cursor so i can continue drawing.
I realize that this could be related to any number of things local to my computer, but thought i would throw it out there in-case it's a SE2D thing.
Looking at CPU usage while waiting for lines to finish shows edge.exe*32 sucking approx. 50%
This is not related to file size and does not effect things like panning.

Cheers
Pete
3 REPLIES

Re: ST4 running slowly

Not applicable
Don't worry guys, problem solved.
I just deleted temp files, and removed a few programs from start up and all good again. I really need to get into the habit of deleting temp internet files regularly cause it catches me every time.
Pete

Re: ST4 running slowly

Not applicable
Does anyone have installation files for ST4.
ST5 will not run in Windows XP pro

Re: ST4 running slowly

Siemens Phenom Siemens Phenom
Siemens Phenom
If you need to reinstall ST4, use the following link.
If you need a different language change ENGLISH to the language needed.
http://free2ddl.ugs.com/pub/SE2DDraftV104ENGLISH.exe