Cancel
Showing results for 
Search instead for 
Did you mean: 

ST6 MP9 issue in Draft>Move

Creator
Creator

A customer is complaining about an issue with the Move command on Draft. Before, he could select the entitites, select the Move command, pick the FromTo point and input a X or/and Y offset, but now, as soon as he picks the FromTo point, the input box for the X/Y offset is greyed out. Did anyone noticed the same problem?

6 REPLIES

Re: ST6 MP9 issue in Draft>Move

Honored Contributor
Honored Contributor

likly one of the selected items is not able to move,

Re: ST6 MP9 issue in Draft>Move

Creator
Creator

I asked the customer to send me the file as I cannot reproduce the problem. He said it was working in MP8 and after install of MP9 it stopped working.

Re: ST6 MP9 issue in Draft>Move

Phenom
Phenom

Your customer has turned on Snap To Grid, on the right side of the Draw group of the Sketching Tab. This will prevent manual key-in of dimensions in the fields for the Move command, among others.

 

Capture.PNG

-Dylan Gondyke

Re: ST6 MP9 issue in Draft>Move

Creator
Creator
Thanks a million, Dylan! That was the solution!

As the customer said it started happen after installing MP9, I would never suspect that.

Again, thank you!

Carlos

Re: ST6 MP9 issue in Draft>Move

Phenom
Phenom
I would have never known, except I did the same thing a few maintenance packs in on ST5 and Ken had to correct me. Smiley Wink
-Dylan Gondyke

Re: ST6 MP9 issue in Draft>Move

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Glad you remembered Dylan because I forgot about that and had no answer Smiley Embarassed



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com