Cancel
Showing results for 
Search instead for 
Did you mean: 

ST6

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

 

    Can we install ST6 on WIN10 64 bit..???

8 REPLIES 8

Betreff: ST6

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @karthik6

 

 

 

have You tried it?

 

 

It could be, that the installtion will work, but I think there is no guarantee for it.

 

What is the reason to stay with ST6?

 

 

regards
Wolfgang

Betreff: ST6

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

one of my customer is using st6 and he asked me whether can he install ST6 on win 10.

 

 

 

Thanks for the reply @hawcad  Smiley Happy 

Betreff: ST6

Phenom
Phenom

I would tell him to avoid Windows 10 unless he absolutely needs it.

For ST6 there is no need for W10.

Biggest mistake I made on my home computer was 'upgrading' from W7 to W10.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Betreff: ST6

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello @hawcad,

 

 

  This is the error he's facing when he try to create a new file ST6 ERROR.JPG

Betreff: ST6

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @karthik6

 

 

 

so if the installation was successful, then it could be that the problem is somewhere else.

 

Let the user change to an admin account adn see wether it will starts or not.

 

regards
Wolfgang

Betreff: ST6

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
It was done with admin rights but still he's facing the error...


. i'll let him know to use on win7 I guess then he can work without any issues



Thanks for the help Smiley Happy


Betreff: ST6

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

in my experience ST7 with the latest MP is "the oldest" version you can sucessfully use on Windows 10.

Anything older (ST6, ST5 etc) will not work on Windows 10, altought they can be instaled on this OS.

 

Ota

Re: ST6

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hey there,

 

Solid Edge is crashing at the startup so I'm assuming it's installed.

Anyways, the reason for crashing is possibly that ST6 is not supported on this OS. You can try running this in comptibility mode for earlier versions of windows and see if it works out or not (try windows 7 or 8).

Officially speaking, it's supported upto 8 only. See the attached excel file below. That will solve all the compatibility questions your customer might have.

 

Regards

Paras Raina

 

 


Paras Raina, Technical Head, MSC Systems Pvt. Ltd. (India)
NX 12.0.2
Solid Edge 2019