Cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 Hole Database

Valued Contributor
Valued Contributor

Whenever I open properties for a hole, I get the warning message:

"Duplicate diameters were found for the same thread family identifier defining threads. Make sure there are no duplicate diameters for the same thread family identifier in the threaded database."

I have opened the excel file and I have looked and looked, but I can find no duplicates. I don't think I have ever modified this database, so I don't understand how there can be duplicates. Is this some known issue? This happens with every standard: DIN, ISO, etc.

7 REPLIES 7

Re: ST7 Hole Database

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you examine all the columns for duplicate diameter values?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST7 Hole Database

Valued Contributor
Valued Contributor
I did. I didn't find any. However I did notice that it only happens on that part file. When I start a new part I don't have the problem.

Re: ST7 Hole Database

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Yes that is a problem in 7. it's due to the new hole.txt. All you need to do when this happen is. Edit the hole/tap, change it size and then change it back. Or delete the hole n the profile anfd apply a new one. By doing this your using the new hole size from the new hole.txt file. This should stop it.

Re: ST7 Hole Database

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Maybe someone can explain what goes on with the \preferences\holes.txt file relative to the \preferences\holes\*.xls files.

 

I changed the ANSI Inch.xlsx file, adding a hole size that was lacking. This thread prompted me to look at holes.txt and I noticed it was modified on the same date as the Excel file was.

 

I don't remember when the Excel files were instituted, ST8 I guess, but does SE still need holes.txt so that it changes it automatically according to what happens in the Excel files?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST7 Hole Database

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

ok, from my take on this. in ST7 i think, they added ANSI Inch.xlsx and removed holes.txt. holes.txt isn't even in my default folder. I just use ANSI Inch.xls. This why you have problem's with old files, the info don't match the new file

Re: ST7 Hole Database

Valued Contributor
Valued Contributor

The problem file was created in ST8.

Re: ST7 Hole Database

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

got me on that, havent it happen since i've cnaged to 8