Cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 - MP2 problem with material API

Gears Phenom Gears Phenom
Gears Phenom

Reading the changelog there is this two statements:

 

PR 1998444: Abort trying to get access to material Table via API
PR 7224772: Old material library APIs do not work for a single material library

 

Well, I wondered what was wrong before cause I never had problems.

 

Now with this MP my usual routine to set a material doesn't work anymore !

 

What should i do ?

 

Dim objMatTable As MatTable
Set objMatTable = objApp.GetMaterialTable
objMatTable.SetActiveDocument objApp.ActiveDocument
objMatTable.ApplyMaterial objApp.ActiveDocument, cMateriale.Text

 

above the code written for V20 that was working in all version up to ST7 MP1

 

Not happy at all

3 REPLIES 3

Re: ST7 - MP2 problem with material API

There are more strange things going on with MP2.
Perhaps they have changed some program code so your macro is not working anymore.
About the code, can't help you. Programming is not my cup of coffee (not a huge fan of tea Smiley Wink ).
-------
Daniël Schuiling

Re: ST7 - MP2 problem with material API

Gears Phenom Gears Phenom
Gears Phenom
I have solved it using the "ApplyMaterialToDoc" method.
It is still a bug in the API to deal with.

Re: ST7 - MP2 problem with material API

Gears Phenom Gears Phenom
Gears Phenom
Not all the bugs comes without a reason.
I found that the "ApplyMAterialToDoc" method is much much faster than the previous one.

So now my program speed is greatly improved.