Cancel
Showing results for 
Search instead for 
Did you mean: 

ST7-MP3: Save as VRML

Phenom
Phenom

Where is this now???

 

2015-01-07 14_14_17-Solid Edge ST7 - Ordered Part - [glijlat nieuw.par].png

2015-01-07 14_14_49-Save As Image.png

 

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
3 REPLIES 3

Re: ST7-MP3: Save as VRML

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What file type are you trying to save, as VRML is a 3D format and isn't available in Draft.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST7-MP3: Save as VRML

Gears Phenom Gears Phenom
Gears Phenom

I'm on ST7-MP3 and the VRML option is still there.

 

Highlighted

Re: ST7-MP3: Save as VRML

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Ken is right, you can create a VRML file only from 3D model.

 

BR,

Imics
http://solidedgest.wordpress.com/