Cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 - Section views

Experimenter
Experimenter

I'm looking to set the revolved section view as a default when placing a section view. Is there a way to do that?

 

 

4 REPLIES 4

Re: ST7 - Section views

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I don't know any ways to set it up as default. This option will be active automatically if your section plane stands more than one segment...

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: ST7 - Section views

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

So if you want that button in by default then you must need to create many drawings with revolved section views.

Could Quick Sheet Templates help?

A section view view in a Quick Sheet Template would retain that attribute.

LMGi
www.TLMGi.com

Re: ST7 - Section views

Experimenter
Experimenter

Yes we do, almost every drawing we create uses the revolved section. I was excited to see quick sheet templates at SEU but with how it works around here. We are more likely to jump from ST7 to ST10 or 11. Looks like I'll just have to deal for now.

 

Thanks

Re: ST7 - Section views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@JasonTitcomb wrote:
A section view view in a Quick Sheet Template would retain that attribute.

So, do you mean she would have to replace the existing file pointed to by the quicksheet via edit links or revision manager?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200