Showing results for 
Search instead for 
Did you mean: 

ST7 & ST8 automatic copy


I do not know if this question has been asked before or not, if so I do apologise.

I have been working on Solid Edge from ST7 (coming from a Autodesk Product)

A one massive problem is the tendency of SE to automatically copy a part when one selects a part/ assembly from the assembly tree, This seems to be more common in big assemblies, can be tedious and make working in the assembly slower. 

Is there a way to switch this off, or in some way avoid it?

It is something SE will need to look at


Re: ST7 & ST8 automatic copy


We also get this in big assemblies and it can be very annoying.

It seems to me that there is some kind of delay and the single click on the pathfinder is registering as a double-click.

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.