Cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 crashes on Win10

Experimenter
Experimenter

Hello,

 

I have the following problem:

I can start ST7 and it loads just fine, when I try to open a file (asm, part, or new file doesn't matter), ST7 crashes. The log file is attached.

 

How can I fix this?

 

Best regards, Simon

4 REPLIES

Re: ST7 crashes on Win10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Open Solid Edge and click the help button.

From there look for the download updates link.

Install the latest update.

I would start with that.

LMGi
www.TLMGi.com

Re: ST7 crashes on Win10

Experimenter
Experimenter

This is what ST7 looks for me. Which help button do you mean? I cannot find one. And sorry the language of the screenshot is not english.

 

Best regards, Simon

Re: ST7 crashes on Win10

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

You have to install Maintenance Pack 4 or newer and it will work well.

 

BR,

 

 

Imics
http://solidedgest.wordpress.com/

Re: ST7 crashes on Win10

Experimenter
Experimenter

Thanks so much @Imics!! It worked, I installed MP8.

Also thanks to JasonTitcomb!

 

What a relief Smiley Happy