Cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 print from DFT with multiple sheets problem

Pioneer
Pioneer

Hi all,

 

When printing from .dft with multiple sheets, and first sheet is in portait position, everything is printing in portrait position, even left sheets are in landscape position.. There is a button "detect landscape/portrait" in options, but it doesnt help Smiley Happy

 

Is it bug or i missed something ? Smiley Happy

 

When saving as PDF, everything is fine, but it is additional step for normal printing.

 

Ignas

3 REPLIES

Re: ST7 print from DFT with multiple sheets problem

Phenom
Phenom

Hi,

 

I had the same problem during the last months and the solution was just installing the last working printer driver.

 

I hope, it will help you too.

 

Yasser

SEST5_MP7

Re: ST7 print from DFT with multiple sheets problem

Pioneer
Pioneer

YD, are you sure?

 

Because, when printing as PDF (not saving as PDF) you are simulating "printer work", it still makes it wrong ?

 

Ignas

Re: ST7 print from DFT with multiple sheets problem

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I agree with Yasser, The printer driver is the culprit.

If Solid Edge can print without problems to one driver - virtual or real printing - it has to work just the same way with any other.

 

~Tushar

www.SurfAndCode.in