Reply

ST8 - Circular Pattern - Pattern - Errors detected - no patterns were created

Hi 

 

I've created a part in Solid Edge ST8, when I try to create a circular pattern I get an error reading "Errors detected - no patterns were created"

 

I've locked the plane to the face and have selected the center point as the base point

 

Please see screen shot attached

 

Any help would be greatly appreciated

 

Thankyou

 

Dominic

3 REPLIES

Re: ST8 - Circular Pattern - Pattern - Errors detected - no patterns were created

Hello Dominic,

Not sure what is going on here. Works OK for me - see the video maybe that will help.

 

(view in My Videos)

Cheers

Mark

Re: ST8 - Circular Pattern - Pattern - Errors detected - no patterns were created

If the hole is an extruded cut (as opposed to created with the hole command) then it looks like you have not selected the bottom of the hole.

Re: ST8 - Circular Pattern - Pattern - Errors detected - no patterns were created

Hi Mark

 

Sorry it's taken so long to reply

 

Your method of selecting the hole from features drop down worked a treat

 

I must have been selecting it wrong as RLR suggested

 

Thanks for the video and the help

 

Cheers