Cancel
Showing results for 
Search instead for 
Did you mean: 

ST8 - Draft - Coordinate Dimensions - Cannot re-orient text.

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Another issue with ST8 (MP03).  Dimensioning in draft environment this time.

 

In a drawing I place some coordinate dimensions (manual not automatic) along a vertical piece of geometry.  I wish to re-orient the numbers to horizontal and execute the command as I have always done but the text does not change!

 

Steps to reproduce:

  1. In a drawing create some coordinate dimensions in a vertical direction.  The text comes in oriented vertical by default.
  2. Select a dimension, right-click <Properties>, and under the <Text> tab set the <OrientationSmiley Embarassed to Horizontal
  3. Click <OK>
  4. The text does not rotate!

 

I have done this a million times on older versions of SE and never a problem.  Does anybody else have this problem?

 

 

 

 

 

Cheers,

 

Chris

2 REPLIES 2

Re: ST8 - Draft - Coordinate Dimensions - Cannot re-orient text.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @chrisstandring,

 

Try going to the "Lines and Coordinate" properties tab.....

 

2015-12-18.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST8 - Draft - Coordinate Dimensions - Cannot re-orient text.

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hi Sean,

 

That works.  Thanks for that.  So it looks like a bit of a change up has been done for reorienting text.

 

 

Cheers,

 

Chris