Cancel
Showing results for 
Search instead for 
Did you mean: 

ST8 MP03 seems slow.

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

I have a colleague who updated ST8 to MP03.  He went straight from the OOTB installation to MP03 skipping the first 2 MP's.

 

He has found some serious speed degradation with MP03 compared to the OOtb installation.  Prior to applying MP03 Solid Edge (OOTB) was fast and responsive, and a pleasure to use.  After applying MP03 Solid Edge has become extremely laggy.  It hangs with just about every command.  It is not so noticeable with single parts or small assemblies, but gets worse with larger assemblies with interpart copies, etc.  I have found the same thing on my machine as well.

 

Can anybody confirm if ST8 MP03 is a lot slower than the OOTB installation?

 

Cheers,

 

Chris

33 REPLIES 33

Re: ST8 MP03 seems slow.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @chrisstandring,

 

 

Not seeing anything notable here........although, having said that, I myself am considerably slower than I was OOTB also!  Robot Embarassed

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST8 MP03 seems slow.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Chris:

 

I also took the same path from ST8 to directly installing MP3 but find no problems.

The computer however has no other worthy software installed besides MS Office and 7Zip, though I am not sure if that is the reason for sailing smooth.

 

The OS is Windows 7

 

~Tushar

Re: ST8 MP03 seems slow.

We have the same problem, but is was also with MP2.

For some reason ST8 is very slow with everything

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: ST8 MP03 seems slow.

Gears Phenom Gears Phenom
Gears Phenom
In assembly when I double click a relation to edit it there is a lag, the edit bar it take a "long" time to appear compared to ST7.

That makes me feel that ST8 is slower.
Highlighted

Re: ST8 MP03 seems slow.

Phenom
Phenom

I didn't notice a difference between one of the MP's.

Only a bit slower in ST8 compared to ST7.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: ST8 MP03 seems slow.

Than I forgot how fast ST8 with no MP and with MP1 was.

 

ST7 was really fast compared with ST8 (at this moment).

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: ST8 MP03 seems slow.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No lags noticed here.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST8 MP03 seems slow.

Creator
Creator

We just upgraded from ST6 MP9 to ST8 MP3 and there is a very noticeable delay with the PMI Dimensioning and Model Views. It seems to take a long time to process/refresh when dimension modification are done on flat patterns in sheet metal. Used to be under a second, now its taking long enough the cursor wait icon appears(2 seconds). Looks like i may be downgrading to the ST8 base release.

 

We do a lot of automation and the overall software is slower then ST6. Previously the system would refresh very quickly, to the point that it could cause seizures. Now the system doesn't even look like there are refreshes happening. Hopefully this can get fixed.

Re: ST8 MP03 seems slow.

Phenom
Phenom
I've noticed a lag in the save time. I have some very simple parts that are taking 20-30 seconds to save. This could be my SSD card but I don't see this type of speed when saving other files (larger files) to the same card.