Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST8 MP03 seems slow.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Dave,


Yes, but there is a ceratin risk, to use those textures by accident without knwoing to use them.

Defining a material with that image defined will slow down SE, isn't it?

 

So I would like to tune the template in such a way, that even there will be no risk to use them some time.

 

Does this mean, I hav eto go to every material, looking which image it uses?

 

 

regards
Wolfgang

Re: ST8 MP03 seems slow.

Siemens Phenom Siemens Phenom
Siemens Phenom

Wolfgang,

 

TBH, I know of no way using the Solid Edge interface to determine what image file is assigned to what material.  I personally would either take the time to open every material and review it for the image file or write a quick program to automate it -- depending on my evaluation on how long each solution would take to accomplish it.  Just because I can automate something, it may still be quicker to do it manually ;-)

 

Regards,

 

-Dave 

Re: ST8 MP03 seems slow.

I will give it a try @uk_dave, thanks for the possible tip.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: ST8 MP03 seems slow.

Gears Phenom Gears Phenom
Gears Phenom

@uk_dave wrote:

Wolfgang,

 

TBH, I know of no way using the Solid Edge interface to determine what image file is assigned to what material.  I personally would either take the time to open every material and review it for the image file or write a quick program to automate it -- depending on my evaluation on how long each solution would take to accomplish it.  Just because I can automate something, it may still be quicker to do it manually ;-)

 

Regards,

 

-Dave 


 

I'm one of those that had performance problem due to missing image files in the past.

To check my assemblies at that time i made a simple vb program (able to also redefine image links).

 

Check this thread: https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Low-performance-issue-in-large-Asse...

 

Francesco

 

Re: ST8 MP03 seems slow.

Creator
Creator

Ran sysinfo, two image files missing:

Images:
Missing:
\\Keyshot\KeyShot 3\Textures\Felt_bump.jpg
[\\Component\Misc\CM004706\CM004706-1.asm]

 

Wouldn't even know what to do to retrieve/replace these.  But to me, doesn't seem like a lot to slow down SE that much.

 

Mark

Re: ST8 MP03 seems slow.

Here:

Images:
  Missing:
  Unused Reference:
    \\emnfs01\engineering\Drawing Files\Projects 2015 - tm\SR\100XXXX - SR 15R 3E with Tensioners\Solid Edge\Textures\Technik\09.jpg
    \\emnfs01\engineering\Drawing Files\Projects 2015 - tm\SR\100XXXX - SR 15R 3E with Tensioners\Solid Edge\Textures\Technik\13.jpg
    \\emnfs01\engineering\Drawing Files\Projects 2015 - tm\SR\Solid Edge\Textures\Technik\09.jpg
    \\emnfs01\engineering\Drawing Files\Projects 2015 - tm\SR\Solid Edge\Textures\Technik\13.jpg
    C:\Program Files (x86)\Solid Edge ST4\images\textures\other\threads.jpg
    C:\Program Files\Solid Edge ST4\images\textures\other\cast_copper_00.jpg
    C:\Program Files\Solid Edge ST5\Images\Textures\Other\brush_steel_00.jpg
    C:\Program Files\Solid Edge ST5\Images\textures\other\cast_copper_00.jpg
    C:\Program Files\Solid Edge ST5\Images\Textures\Other\cast_steel_00.jpg
    C:\Program Files\Solid Edge ST5\Images\Textures\Other\GOLDEN_1.JPG
    C:\Program Files\Solid Edge ST5\Images\textures\other\threads.jpg
    C:\Program Files\Solid Edge ST5\Images\Textures\Other\weldbeads.jpg
    C:\Program Files\Solid Edge ST8\Images\Textures\Other\weldbeads.jpg
    C:\Program Files\Solid Edge ST8\Images\textures\wood\wood_1.jpg
    N:\Cool parts\Poppen\POPPEN\PP-Face.png

 

These textures are not even used in the material table. How do I fix this? And I know that they are not missing, but how do I fix the unused references?

 

Even the first few have never an image in them. What is going on?

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: ST8 MP03 seems slow.

Does anyone know if there is a purge function, like in ACAD, in SE?
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: ST8 MP03 seems slow.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Francesco

 

Hi, great tool, but is it possible to either provide the code or to change it in that way, that also parts and psm could be checked

 

thanks and regards

 

 

regards
Wolfgang

Re: ST8 MP03 seems slow.

Gears Phenom Gears Phenom
Gears Phenom

@hawcad wrote:

@Francesco

 

Hi, great tool, but is it possible to either provide the code or to change it in that way, that also parts and psm could be checked

 

thanks and regards

 

 


 

It already does check also parts and psm; if you want the code write me a PM with your email and i will send it to you.

 

Francesco

Re: ST8 MP03 seems slow.

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

GTAC have been able to reproduce the problem and are working on it.  PR7609395.