ST8 Out Down Grade..

Pioneer
Pioneer

ST8 Etch feature cramping.
I want to go back to st7 or st6.

thereby clear the file saved to a st8
Anything can go to a lower version? ...

What should I do? ...

3 REPLIES

Re: ST8 Out Down Grade..

Esteemed Contributor
Esteemed Contributor

Hi there,

 

Solid Edge, much like other CAD software, is not backward compatible.....so you're only option there would be to export to a neutral [Parasolid, or similar] format, and re-import into the lower SE version. You may loose some/all of the etching information though.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ST8 Out Down Grade..

Pioneer
Pioneer

I also like the SOLID EDGE.
But, the bug can not understand.

The release of this feature does not work well when a new version.

And wait til MP to make.

What right does not, right? ... Well the release of an existing function inde ...

Re: ST8 Out Down Grade..

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Have you reported the issue? If others are having similar issues it maybe easier for GTAC to isolate the source if they have more test cases...

 

Perhaps others here on ST8 could replicate your workflow to generate the same issue?

Shane Murray
ST10 MP2