Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

ST8 REVISION MANAGER - ADDING REVISION NUMBER

Legend
Legend

I'm copying a psm and draft, and when changing number from 01 to 02, it is kind enough to make my revision 02 without even asking.

 

Why?

 

Capture.JPG

ST8 MP9
Go FAST, or go home.
6 REPLIES 6

Re: ST8 REVISION MANAGER - ADDING REVISION NUMBER

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And you're not using Insight?

I see three places where there's an 02. Which one did you change and which changed automagically?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST8 REVISION MANAGER - ADDING REVISION NUMBER

Legend
Legend

I copied my draft and psm, from -01 to -02, not using Insight, and SE was kind enough to go ahead and claim my new draft and psm are now revisions -02. The original 01's had no revision before being copied.

ST8 MP9
Go FAST, or go home.

Re: ST8 REVISION MANAGER - ADDING REVISION NUMBER

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm going to assume it's because you named the files with the suffix -02, which fits Edge's default naming convention for revisions. I think you can use - or _ as revision delimiters.

The help isn't informative on the limits of what can constitute a delimiter. Surprise!

 

revisionsettings.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST8 REVISION MANAGER - ADDING REVISION NUMBER

Legend
Legend
Well, isn't that CUTE! Okay, changed the options, problem solved. Thanks for the help!
ST8 MP9
Go FAST, or go home.

Re: ST8 REVISION MANAGER - ADDING REVISION NUMBER

Experimenter
Experimenter

Is there a way to stop Solid Edge from automatically filling in that Revision column? When I use revision manager to copy a .psm and .dft it fills in the revision column automatically(in this case "G3393PA") based on the new file name and I have to delete it EVERY time which is annoying.  Never happened when i used ST6

 

SE.pngSE2.png

 

 

 

 

 

Re: ST8 REVISION MANAGER - ADDING REVISION NUMBER

Experimenter
Experimenter

Wow of course I figured it out 2 minutes after making a post on here

 

I set the "Revision Delimiter" value to a period "." instead of a dash "-"