Showing results for 
Search instead for 
Did you mean: 

ST8 Win10 Font


OK. I'm helping someone running ST8 on a Surface Book with Win 10 OS. He has his Surface resolution set down to 1920 X 1200 and has the Win 10 Scale for text, apps and other items set to 200% which is the Recommended value.


When we open ST8 the Prompt bar text is tiny! Since this is the haven of the Solid Edge gurus I was hoping someone could provide and answer on how to adjust the prompt line to something readable.




Betreff: ST8 Win10 Font

Esteemed Contributor
Esteemed Contributor

HI @RyanM




have You tried to change the option in the Helpers tab of Solid Edge Options?



I have seen, that with ST10 there is no button active anymore, but maybe with the ST8?



Re: ST8 Win10 Font

I hate do this but I found my own answer! I didn't realize that at the far right was some controls! One is Increase font! I didn't know about this until I changed my theme to "Some Assistance" and it resized and relocated the prompt bar then I noticed the controls!

Someone one to do a quick reply and I'll and give the points for an answer?