Cancel
Showing results for 
Search instead for 
Did you mean: 

ST8 crash at hole creation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

I got reported a crash situation with ST8 (MP4-6) several times
when users are going to create holes in sequential environement.

 

After places hole circles and closing the layout/sketch environment a crash/crashlog appears.

 

This doesn't be every time but several times a day on different workstations for different users.

 

Has anybody else seen this behaviour too?

 

 



regards
Wolfgang
2 REPLIES

Re: ST8 crash at hole creation

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, I've seen some similar situations. User had a basic AMD (ATI) graphics card and he used textures and all visual settings (reflection and etc...) after suppressing all Solid Edge had been more stable... Ugly AMD graphics card! Smiley Very Happy

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: ST8 crash at hole creation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hallo IMics,


thanks for that answer.

This is confirming that behaviour and maybe the hint with the graphic will bring us further on investigating the problem.

 

by the way, AFAIK there are only nVidia cards used.

But they also had problems for the last couple of month and this has to do with that too.

 

 



regards
Wolfgang