Cancel
Showing results for 
Search instead for 
Did you mean: 

ST8 on Win7 with MP6 crashes by icnt.exe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edegrs,


can anybody confirm that with ST8 and MP6 on Win7 the icnt.exe (Insight Connect, Revision Manager)  is not able do start and brings an error message.

 

It also might have to do something with the JUtil.dll

 

And I have seen that both files will be updated with the MP6

 

It is no problem with Win10 operating system, only on Win7 machines

 

 

PS.: it seems that the Keyshot app also makes similar problems and is not able to start after MP6 where it was possible before

 

A deinstallation of MP6 and MP5 with a new installation of MP5 solves the proplem

Maybe this can help to find out the reasons.

 

Thanks in advance for any hints and tipps

 

 

regards
Wolfgang
5 REPLIES 5

Re: ST8 on Win7 with MP6 crashes by icnt.exe

Legend
Legend

Hi Wofgang,

I have only tried to open an assembly in revision manager and copy it to another location and seems to work correctly.

 

Best regards

 

Héctor Pelayo Izquierdo
Engineering Department, JAE Ingeniería y Desarrollos, S.L.
Solid Edge ST9 MP5 | NX 9
Development: VB.NET

Re: ST8 on Win7 with MP6 crashes by icnt.exe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Hector,


thanks for the info.
The error message also comes up if only starting ICNT.exe from win32 directory of Solid Edge

So there is no need for any file or document to be opened


regards
Wolfgang

Re: ST8 on Win7 with MP6 crashes by icnt.exe

Gears Phenom Gears Phenom
Gears Phenom

Here no problem to start icnct.exe alone or by right click open revision manager on a solid edge file.

 

ST8 MP6 on Win7 

 

Re: ST8 on Win7 with MP6 crashes by icnt.exe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Fiorini,


thanks for that info.
Assure me in my opinion, that it should be something coming more from that computers than from SE or MP itself
regards
Wolfgang

Re: ST8 on Win7 with MP6 crashes by icnt.exe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No problems here...

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200