Cancel
Showing results for 
Search instead for 
Did you mean: 

ST8 wont appear as default program

Builder
Builder

When navigating my Window's File Explorer I cant open a STEP file with Solid Edge. The only thing SE related is the viewer. And when I try and find SE using the browser I cant select it.

 

I use to be able to open STEP files from the File Explorer with ST7, but it would always open another instacnce of SE. If possible I would like to be able to open STEP's from the File Explorer into my current instance of ST8.

 

Thanks,

SW 

5 REPLIES

Re: ST8 wont appear as default program

Siemens Phenom Siemens Phenom
Siemens Phenom

This is covered in GTAC Solution Center article 002-7004559:

 

http://solutions.industrysoftware.automation.siemens.com/view.php?si=002-7004559

 

The registry file to accomplish this can be downloaded from my personal GitHub site:

 

https://raw.githubusercontent.com/uk-dave/SolidEdge/master/open_step_in_solid_edge.reg

Re: ST8 wont appear as default program

Builder
Builder

Thank you for the quick response and info. But what do with these registry keys? Or where do I insert them?

 

Thank you

Re: ST8 wont appear as default program

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave,

How does one download your .reg link? All I get is a window full of text. Copy and save it as a .reg file (if possible) then import while in regedit?

But if it's a script that doesn't seem right so I'm not sure how to use it.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: ST8 wont appear as default program

Siemens Phenom Siemens Phenom
Siemens Phenom

If your browser is displaying it as text, simply right click over the window with the text and select "Save As…" [Chrome] or select all the text and copy and paste it into notepad and save as to a registry file [.reg extension].  Then simply double-click on the saved .reg file to install it.

Re: ST8 wont appear as default program

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave Thanks. I was clueless (obviously). Wasn't sure you could simply save .txt as .reg and it would work. Nor did I know you could save the window like that.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200