Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 Assembly relations - flip as default

Valued Contributor
Valued Contributor

Dear Experts,

 

All the time we have an annoying problem when add relations between two bodies. Its faceing two faces but opposite sides!

Is there a chance to flip this choice once for good rather than clicking all the time? Smiley Sad(( It is ridiculous.

 

Thank you for chance to live better with this tool.

4 REPLIES 4

Re: ST9 Assembly relations - flip as default

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you post a picture or example of what you are trying to accomplish to help better understand?

Re: ST9 Assembly relations - flip as default

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

You can try using Capture Fit from the 'Assemble - Options' dialog when assembling. It will position the part correctly everytime. See attached image.

 

 

Re: ST9 Assembly relations - flip as default

Gears Phenom Gears Phenom
Gears Phenom

capture fit as was recomended...

 

or

 

drag parts so that the faces being mated are closest to on another and orientated corrected...

 

I beleive the solver is simply trying to make the relationship by moving the componants the min distance...

 

one you model long enough you simply get used to using the flip command...   dont forget you can do this while making the relationship!!!   read your prompt bar for tips...


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7
Highlighted

Re: ST9 Assembly relations - flip as default

Honored Contributor
Honored Contributor

If you are using mate as the default for plane mates, Use planer aligned instead. 

 

Mate by default, has the normals face each other

Planer align be default, has the normals the same direction