Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 Crash on selecting sketch plane.

Experimenter
Experimenter

Win 10 has just done an update and right after that SE ST9 crashes when I try to select a plane to sketch and extrude in ordered  mode. It crashes in syncronous mode too, when i try to select the initial point to extrude a box.

I attach the .txt crashlog file.

 

Thanks in advance.
Regards.

3 REPLIES

Re: ST9 Crash on selecting sketch plane.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Looks like the graphics card driver might have an issue.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST9 Crash on selecting sketch plane.

Experimenter
Experimenter

Just done the automatic win 10 driver update and nothing changed. Any idea on how to solve it is wellcome.

Re: ST9 Crash on selecting sketch plane.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Generally the Windows drivers for hardware aren't usually that great.  In the case of a Graphics card, you typically have to go to the manufacturer (NVIDIA, AMD, INTEL) to get the latest driver for your model.  If you have a laptop (HP, DELL, LENOVO) you need to go to them to get the latest driver for your graphics card.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com