Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9: DXF export

Experimenter
Experimenter

Dear community,

 

please help me with setting an export to DXF file. The drawings are simple 2D as contour for cutting machine. The machine can load DXF files but have problems with "complex" entities like INSERT, NURBS, SPLINES etc. Is there a way how to export DXF file which not have INSERT blocks, but only entities like LINES, ARCS, POLYLINES? 

 

Thank you.

SpaM

7 REPLIES 7

Re: ST9: DXF export

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Try to manipulate the save options to  DXF.

When you use "Save as", select .dxf and Options. There you'll find some options to turn the dft to dxf. 

Re: ST9: DXF export

Experimenter
Experimenter

I installed trial ST9 but can not find "save as DXF" option. Do I need to install something else?

 

Thank you. 

Re: ST9: DXF export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
  1. Save As or Save As Translated.
  2. Change Save as type: to "AutoCAD documents (*.dxf)"
  3. Select Options button

 

 

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST9: DXF export

Gears Phenom Gears Phenom
Gears Phenom

Really, you shouldn't save out the drawing as dxf for programming a cutting machine. YOu should be in the sheet metal environment and save as dxf from there.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: ST9: DXF export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @SpaMBX001,

 

What build & version of Solid Edge are you using?.....if using Free2D, then you're i bit stuck, but,  if you're using one of the full commecial 3D builds, [Foundation, Classic, Premium] then the only place that has this control, is from the Sheet Metal environment specific "Options", where there is a check box to allow the user to "Simplify b-splines". Attached are the flat pattern DXF files from a very basic sheet metal part, but shows it in both states.

 

ST9_PSM_FlatPatternTreatments.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST9: DXF export

Experimenter
Experimenter

I do not have "AutoCAD documents (*.dxf)" option in ST9. 

Re: ST9: DXF export

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@SpaMBX001, What module are you in... Draft, Part, Sheet Metal?

 

If you are not in Draft, then you will not have that option as you are in a 3D environment and it does not export to a 2D DWG or DXF.

 

If you are in Sheet Metal, then you can use the "Save As Flat" command which uses the options that @SeanCresswell mentioned and should give you clean geometry but your model must be created using the sheet metal commands I believe to be able to use this command.  If just 2D, then use the Tab command to create it.

 

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com