Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST9 Detail View Boundary Bug?

Phenom
Phenom

@Tushar - We are using ST7

If we rotae a view then create a detail view from that everything is OK.

If we then make it an independant detail view it disappears.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.
Highlighted

Re: ST9 Detail View Boundary Bug?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Unable to verify these steps with ST 8 MP 9 or in ST 9

Do you have the latest MP for ST 7 though I have no information if it is fixed in ST 7

Re: ST9 Detail View Boundary Bug?

Phenom
Phenom

@Tushar - using MP11 (I need to change my info on here !)

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: ST9 Detail View Boundary Bug?

Valued Contributor
Valued Contributor
Beachcomber I've noticed that also since I started using SE in ST7.

Re: ST9 Detail View Boundary Bug?

GTAC says this issue will be fixed in ST10. Until then, there is a workaround. Select CTRL+SHIFT > Update Views to regenerate the view correctly.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10