Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

Hello everybody,

 

it is some time now that after a while (less than 2 hours) some Solid Edge dialog windows starts to appear very slowly.

They do appear that slow that you are able to see each icon being drawn.

I toke a video to show that.

 

Anyone experienced the same behaviour ?

 

Restarting Solid Edge fix the problem for a while then it start to slow down again; the more I wait to restart the more it get slower.

 

(view in My Videos)

151 REPLIES 151
Highlighted

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Fiorini  I have not seen that and we run ST9 on over a 100 PC's.  I'm assuming you have your graphics driver up to date...

 

What are your PC specs?

(OS, Memory, Graphics)



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

Win 10, 16Gb, K2200

 

I got the problem since MP09 but can't be sure to blame it or other things.

My co-workers are on Win 7 and haven't got this problem.

 

Edit: I feel like it started with the Fall Creator Update of win 10

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We don't have the Fall Creator's Update installed yet.  That could be a reason but hope not...  Have you attempted to update your graphics driver since that installed?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@KennyG wrote:

We don't have the Fall Creator's Update installed yet.  That could be a reason but hope not...  Have you attempted to update your graphics driver since that installed?


Not yet, I am going to update them next

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@Fiorini wrote:

@KennyG wrote:

We don't have the Fall Creator's Update installed yet.  That could be a reason but hope not...  Have you attempted to update your graphics driver since that installed?


Not yet, I am going to update them next


I just checked and I am on quite new driver version 382.05 where the latest are 385.69; I usually don't update graphics drivers unless problems, I may try to switch back to the old 36x.xx

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What's the build number on the fall creators update so I can check?

Haven't noticed the problem.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

Version: 1709

OS build: 16299.19

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm still on 14393. It would be worth knowing if the update is the reason. If for no other reason to avoid it.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@Fiorini wrote:

@Fiorini wrote:

@KennyG wrote:

We don't have the Fall Creator's Update installed yet.  That could be a reason but hope not...  Have you attempted to update your graphics driver since that installed?


Not yet, I am going to update them next


I just checked and I am on quite new driver version 382.05 where the latest are 385.69; I usually don't update graphics drivers unless problems, I may try to switch back to the old 36x.xx


Latest driver didn't solve the problem.

I must say that the problem occours not by how much time Solid Edge is open.

It is something strange, sometimes I close Outlook and Solid Edge starts to work good again, sometimes not.

 

I will re-install it next week and see what happens