Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@Fiorini wrote:

@Ninth-Inning wrote:
Just curious, did you do a reboot of your PC after installing the MP?

No I didn't reboot; I will tell later today how Solid Edge behave.


Problem still there after the reboot.

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@RDH wrote:

Today Microsoft indicated the fix is in. Here is the KB info. I don't see an explicit mention of the GDI memory issue but I didn't follow all the links.

 

https://support.microsoft.com/en-us/help/4058258/windows-10-update-kb4058258


I have just installed this KB (Manually donwloaded) and I must say that first tests are really promising.

Everything is back to fly... will tell later today if the good performance stay there or degrade while time pass.

 

Finger crossed

Re: ST9 Dialog windows slow down

Valued Contributor
Valued Contributor

After a short test I can confirm that this update solved the issue.

SE2019 MP3

Re: ST9 Dialog windows slow down

Creator
Creator

I can confirm, as well that on ST10, this patch works quite well.  Night and day.   I have a couple fairly large draft files that like to build the issue really fast, but they operate just fine.  In fact, it appears that the draft file actually opened a bit faster itself as well.  Didn't take nearly as long to populate the sheets as it did previously.

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks @RDH,

 

Initial use......is as good as others are reporting. "Night & Day".

All in all, a great result. I'll run it for a few more hours before I load it onto my collegue's PC.

 

Thanks to the SE team for the perseverance in countering this.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: ST9 Dialog windows slow down

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I just installed the update and I'm seeing much quicker response in the callout dialogue box.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: ST9 Dialog windows slow down

Experimenter
Experimenter

The KB worked for us as well, unfortunately I'm having the same trouble again since the last Windows update... Reinstalling the KB won't do the trick. Any new idea's?

Re: ST9 Dialog windows slow down

Siemens Genius Siemens Genius
Siemens Genius

What is this "new windows update"?

Re: ST9 Dialog windows slow down

Experimenter
Experimenter
I had a (minor?) automatic update last week

Met vriendelijke groet,

Jos Buschgens | Chief Engineering

[Denta Engineering]


DENTA Engineering Molenstraat 138
3764 TJ SOEST

T +3135-6022992
M +316-22660186
jos@denta.nl

Re: ST9 Dialog windows slow down

Siemens Phenom Siemens Phenom
Siemens Phenom

@Jos_Buschgens there are two types of Windows 10 updates -- Feature updates and Quality updates.

 

Regardless of which type of update, you should really review your Windows 10 Update policy and consider explicitly delaying Windows 10 updates:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/Let-s-talk-Windows-10-and-Feature-Up...