Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST9 Dialog windows slow down

Creator
Creator
If your intent is to show/hide right click in the part/assy name then select either the show or hide option in the pop up menu - which are the top 2 choices. Right clicking on the check box will do nothing. It's not ideal adding an extra click, but it does same from having to remove added parts or assemblies at random. I know it's frustrating. Always happens when it's most inconvenient.

Re: ST9 Dialog windows slow down

Innovator
Innovator
@Ninth-Inning

Ahh, ok. Gotcha. Yes, I have not noticed or experienced any "part drag" problems with that workflow. It is only when I use the check box to show or hide.

Thanks for the feedback Ninth-Inning!

Brian C.