Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST9 Dialog windows slow down

Legend
Legend
See same behaviour after update of windows 10 to the fall creators update... I'm on ST10 MP2

Are more users having this problem with the latest Windows 10 update ?

Kind Regards,


Jan Bos
Emmen, the Netherlands
User since V3.5

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, just updated Win 10 to version 1709 and now seeing the same thing...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: ST9 Dialog windows slow down

Legend
Legend

Hi,

Searched for beta drivers from Nvidia.. this is what they wrote in the latest QNF driver;

Additional Notes
This release is targeted towards early adopters of Windows 10 Fall Creators Update. General deployment is recommended with the next Optimal Driver for Enterprise (ODE) release.

And from another source;

The official launch NVIDIA GeForce display driver for Windows 10 Fall Creators Update is 387.92. Please make sure your PC is using driver 387.92 or newer. You may download the latest NVIDIA display driver from our software downloads page:

The WHQL or recommend driver that are displayed with the regular search are older and do not have the fixes for the Fall creator update..

 

http://www.nvidia.com/Download/Find.aspx?lang=en-us


Will test the latest QNF driver 388.16 on monday... I hope this will fix this problem.

Kind regards,


Jan Bos

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom
Thanks for the informations @Jan_Bos I'm going to try the QNF now

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@Fiorini wrote:
Thanks for the informations @Jan_Bos I'm going to try the QNF now

I can confirm that with the 388.16 driver version the problem is still present

 

Are we sure that it is a driver problem ?

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Fiorini

 

 

 

can You post Your hardware specifications?

 

Are You sure that SE is using Your graphics card rather than working with an onboard graphic?

This is one of the most frequently reasons for a performance problem with SE.

 

 

 

regards
Wolfgang

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@hawcad wrote:

Hi @Fiorini

 

 

 

can You post Your hardware specifications?

 

Are You sure that SE is using Your graphics card rather than working with an onboard graphic?

This is one of the most frequently reasons for a performance problem with SE.

 


HP Z240 Workstation

 

Intel Core i7-6700 3.4GHz

8 GB RAM

nVidia Quadro K2200 4Gb

 

Quadro card is the only video adapter installed

 

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Fiorini

 

 

 

but now I'm a litte confused.

 

Before You spoke about a Gforce graphics card and now there is a Quadro installed.

So do You have the right drivers, etc.

 

 

regards
Wolfgang

Re: ST9 Dialog windows slow down

Gears Phenom Gears Phenom
Gears Phenom

@hawcad wrote:

@Fiorini

 

 

 

but now I'm a litte confused.

 

Before You spoke about a Gforce graphics card and now there is a Quadro installed.

So do You have the right drivers, etc.

 

 


I never mentioned GeForce cards

Re: ST9 Dialog windows slow down

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Jan_Bos schrieb:

Hi,
...


The official launch NVIDIA GeForce display driver for Windows 10 Fall Creators Update is 387.92. Please make sure your PC is using driver 387.92 or newer. You may download the latest NVIDIA display driver from our software downloads page:

...


Jan Bos


Hi @Fiorini

 

 

I was confused and concentrated by/to this post

regards
Wolfgang