Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 FILE IS CORRUPT

Experimenter
Experimenter

Estou tentando há dias, instalar o ST9, não consigo, arquivo corrompido EXTRACTION FAILED, FILE IS CORRUPT. Alguém pode me ajudar?

1 REPLY 1

Re: ST9 FILE IS CORRUPT

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @SANDRA1,

 

The file is very large [2.85GB] single package [.EXE] file, that needs to be complete in order to function correctly.

Do you have a fast & stable internet connection, also, what web browser are you using to download the file, as you might try using a download manager, such as "Chrono" for Google Chrome, as it will greatly assist in obtaining a complete file download, with any transmittal interuption[s].

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000