ST9 License Manager Downward Compatibility

Creator
Creator

With plans to upgrade from ST6 to ST9 in 2017, preparations are being made to upgrade the current SE license manager on our license server to the LM version provided with ST9.

 

As we will continue to use ST6 for some time before upgrading to ST9, the question is if ST6 will be compatible with the ST9 based LM?

6 REPLIES
Highlighted

Re: ST9 License Manager Downward Compatibility

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, ST6 should run just fine with the FlexLM server delivered with ST9 and an ST9 license file.

Re: ST9 License Manager Downward Compatibility

Esteemed Contributor
Esteemed Contributor

We are running ST6 with the ST9 license server.  No issues.



Ken

Production: ST10 MP3
Testing: SE 2019

Re: ST9 License Manager Downward Compatibility

Creator
Creator

Thanks for confirming Ken.

Re: ST9 License Manager Downward Compatibility

also, be advised that you can do a dual install... I have ran ST9 on top of ST6 without issue.
===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6

Re: ST9 License Manager Downward Compatibility

Creator
Creator

Would you recommend the complete uninstall of the ST6 based LM prior to the install of the version that came with ST9?

 

The files appear to install in the same location - C:\SEFlex\Program\.

Re: ST9 License Manager Downward Compatibility

Siemens Phenom Siemens Phenom
Siemens Phenom

If it were my systems, I would uninstall the old version first.