Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

ST9 - Multibody part - different material

Phenom
Phenom

I have designed a part of foam.

Now I've been asked to make the 2 sides in a stronger foam.

So I created 2 planes and made a split to have a multibody part.

When I change the material, the material of all 3 bodys change.  

Can this be different? How?

 

Thanks!

...........................................................................................................
Solid Edge 2020 & AutoCAD 2020 user
14 REPLIES 14

Betreff: ST9 - Multibody part - different material

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

 

 

 

as this was discuseed a couple of days ago, NO, one part = one material

 

But - as there always is a "but" - after separating those 3 parts into 3 separate part files, of course associative, You can change these materials for those individual part childs.

 

 

regards
Wolfgang

Betreff: ST9 - Multibody part - different material

Phenom
Phenom

Thanks for your answer, but:

PFFffff....

 

...........................................................................................................
Solid Edge 2020 & AutoCAD 2020 user

Re: ST9 - Multibody part - different material

Gears Phenom Gears Phenom
Gears Phenom

I think i recalling hearing something in the ST10 release that there were improvemets to Multi part...

 

Maybe Different Sheet metal Gauges?  maybe multi Material???

 

@DavidChadwick or @LauraWatson   can either of you expand on the whats new for Multi Body in ST10, if any?

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: ST9 - Multibody part - different material

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Re: ST9 - Multibody part - different material

Siemens Genius Siemens Genius
Siemens Genius

Matt - what I see in ST10 is more in the area of better tools to create a "one body assembly" from an assembly. So maybe the workflow suggested to create an assembly of individual parts and then create a one body assembly from it when needed wll be the way to go in ST10. Some reasons to do this might be to remove design details and protect your IP if you need to send out your design to a 3rd party, or to improve performance in large assemblies,

Dave

{David Chadwick}, {Solid Edge Portfolio Development}, {Siemens PLM Software}

Re: ST9 - Multibody part - different material

Valued Contributor
Valued Contributor
Not much of a hardship to publish the assembly and assign the correct materials is it? They are still linked to the parent part so you can still edit in context if needed. I think your Pffffttt is lazy drafting/modelling if I'm honest.

CAD/CAE Manager
SE2019 MP5

Re: ST9 - Multibody part - different material

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Guy_H77

 

 

 

this is the same I'm thinking about!

After modelling the master aprt with multiple bodies in it, press the "Multi-Body Publish" button and that's it.

Changing individual material within the childs, which also is not a real hard work to do.

 

regards
Wolfgang

Re: ST9 - Multibody part - different material

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So I guess there's something wrong with asking for more features so you can do things a certain way rather than another. A way that you might think is more efficient. Assemblies take more overhead. Not a great amount usually but for me if I don't need an assembly for documentation purposes I'd rather only have to deal with one file. So sorry.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: ST9 - Multibody part - different material

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

After you publish use Property Manager to set the materials.

LMGi
www.TLMGi.com