Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 Multiple Monitor issues

Gears Phenom Gears Phenom
Gears Phenom

ST9 MP4

 

Anyone seeing Multiple Monitor issues.

 

Any fixes, work arounds, or IR filed?

 

Historically I recall Variable table being a window that might "stick" to a secondary monitor and not be accessable once only using 1 monitor.  But with ST9 im feeling like there are a lot of windows and pop ups that are not honoring SEApp space properly.

 

For Example:

1)  I launch SE on main monitor, move SEApp to 2nd moitor then close SE.  When i relaunch SE, the splash screen opens on Main moitor but SEapp opens on 2nd monitor.

2) If I open a Recenly used file while SE is on teh second monitor and the file opens as readonly...  the Read only assistant does not display at all.  i can not write to the file.   but if i drag SEApp to main monito then the read only assistant is now visable and i can edit my file.

3) SEapp on monitor 2, materail opens on main...

others...

 

anyone else seeing such behavors?

 

 

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7
14 REPLIES
Highlighted

Re: ST9 Multiple Monitor issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hey @Johnson_BigMatt,

 

Now that you mention it, I've seen a sort of similar issue.

....on my ext monitor I run two applications, Solid Edge & Excel, with everything else being on the Surface Pro3 screen.

If I move a dialogue box [which I now no longer do] on the ext monitor, then when I use SE out of the office [ie: disconnected from the dock] it is floating off screen and waiting for input, so SE is locked....forcing me to task manager close it out, until I can dock it again to correct the dialogue box set out. [usually offender is the Material Properties, which I use set to prompt at new model creation]

 

I find my system remembers the last used monitor settings OK, but I just have to make sure not to move anything BUT the main application window to the ext monitor. No reports of this from my other user.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST9 Multiple Monitor issues

Gears Phenom Gears Phenom
Gears Phenom
IR 7953891 has been converted to ER 7953891; Desc: Dialogs do not follow application to secondary monitors

Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: ST9 Multiple Monitor issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

7 of us have dual monitors and I haven't heard of any complaints. I did try what I think matches your scenario: Open SE in main, move to second, close SE, open SE with splash on main but SE on second, open read-only recent file, and read-only box is on second and accessible.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: ST9 Multiple Monitor issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MattJohnson_PG wrote:
IR 7953891 has been converted to ER 7953891; Desc: Dialogs do not follow application to secondary monitors

 

Have asked my VAR to append us to this ER.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST9 Multiple Monitor issues

Genius
Genius
In this situation where your dialog box is on the 2nd monitor and you can't access it, have you tried to Alt+Spacebar then M to move the dialog with the arrow keys? I have run into this a time or two.
Dale Smith
Mitsubishi Electric Power Products, Inc.
ST10 MP7 - Insight

Re: ST9 Multiple Monitor issues

Gears Phenom Gears Phenom
Gears Phenom

Thanks Dale.  Great tip, also Windows button + Right Arrow works well...

 

But was hoping for a root cause or reg hack to reset globally...

 

seeing numerous issue.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: ST9 Multiple Monitor issues

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Matt,

 

I have floating dialog issues with my Surface Pro 3 (with Windows 10) and a 2nd monitor attached through the docking station.  It's not Solid Edge specific, though.


____________________________________
--Scott Wertel, P.E.

Re: ST9 Multiple Monitor issues

Valued Contributor
Valued Contributor

We have a user that has an Apple Cinema Display coupled with an HP ZDisplay running off of an NVIDIA Quadro K200.  Since upgrading to ST9, Solid Edge no longer highlights the parts while hovering over them.  If he takes off the Cinema Display off of the System that function returns.  He had no issues with ST8.

Re: ST9 Multiple Monitor issues

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

@mdamson, that sounds like your hitting the wall with the performance of your graphics card, which is why turning off excess graphics features restores functionality.

 

With respect to @Johnson_BigMatt 's problem, I honestly wonder if this is a Solid Edge issue or a larger Windows 10 issue.


____________________________________
--Scott Wertel, P.E.