Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: ST9 Multiple Monitor issues

Gears Phenom Gears Phenom
Gears Phenom
We are running Win 7, multiple workstations, laptop and desk top, different graphic cards. but can reproduce with consistency... currently with ST9 M4 with SEEC, but same behavior in managed and un managed modes...
Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7
Highlighted

Re: ST9 Multiple Monitor issues

Gears Phenom Gears Phenom
Gears Phenom

@Johnson_BigMatt, well that definitely narrows it down.


____________________________________
--Scott Wertel, P.E.

Re: ST9 Multiple Monitor issues

Gears Phenom Gears Phenom
Gears Phenom

@swertel wrote:

@mdamson, that sounds like your hitting the wall with the performance of your graphics card, which is why turning off excess graphics features restores functionality.

 

With respect to @Johnson_BigMatt 's problem, I honestly wonder if this is a Solid Edge issue or a larger Windows 10 issue.


The perceived feeling of ST9 compared to ST8 it is an overall loss of performance.

Looking at all the complain about ST9 should raise the attention on what's happened.

 

In my everyday workstation I still have Windows 7, so there must be something in ST9 too and not just on Windows 10.

Re: ST9 Multiple Monitor issues

Genius
Genius

Sorry meant to post a NVIDIA Quadro K4200.  So, I don't think we are hitting the limit of the card.

Re: ST9 Multiple Monitor issues

Honored Contributor
Honored Contributor

I have a K4200 and it "runs out of gas" about every 3 hours of use. Reboot!