Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 - RMB on pathfinder during edit in place of a feature doesn't work

Gears Phenom Gears Phenom
Gears Phenom

I'm 99.9% sure that right clicking a part on pathfinder during editing in place of a feature of another part was working prior to ST9.

 

Steps to reproduce

1.Open an assembly

2.Edit in place a part

3.Edit or create a feature

4.During the feature sketch step right click a part on pathfinder and nothing happen

 

Why I do this ? To activate\show\hide\shoe planes\ etc.etc.

 

Confirmed ?

 

Still disappointed of ST9

4 REPLIES 4

Re: ST9 - RMB on pathfinder during edit in place of a feature doesn't work

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I can confirm this.

In ST8 when you edit sketch of a part feature and your part is opened in IPA mode, you can RMB click on other part in assembly to show context menu. In ST9 RMB this does not work.

 

This should be logged to dev. as a regression from ST8.

 

Ota

Re: ST9 - RMB on pathfinder during edit in place of a feature doesn't work

Gears Phenom Gears Phenom
Gears Phenom

IR 7939113 filled.

 

Feel free to add you voice to this IR to escalate priority

 

 

Highlighted

Re: ST9 - RMB on pathfinder during edit in place of a feature doesn't work

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thanks for IR number, I will join you.

 

Ota

Re: ST9 - RMB on pathfinder during edit in place of a feature doesn't work

Community Manager Community Manager
Community Manager

@Fiorini

@ota_poul2

 

I've added this PR to weekly Change Control Board (CCB) meeting. 

Development is taking a look now.

 

Laura