Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 - Replace background - default file

Gears Phenom Gears Phenom
Gears Phenom

When replacoing a background in ST9 draft SE looks in the SE default template file, even if you change the draft file path in your options. 

Also SE doesn't remember your last path where you searched for a teplate background sheet...

 

Our VAR explained me were I could change the default path for a backround change, it is somewhere hidden in the windows register, but for some unknown reason that setting is lost...

 

I don't want to bother our VAR again, does somenone here know were I can change that?

xbwZ3E9

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
10 REPLIES

Re: ST9 - Replace background - default file

Phenom
Phenom

You would have thought it would use the User Templates location in the file locations tab of SE settings, but it doesn't appear to.  This might have been what your VAR was thinking of?

 

I don't know of any registry hacks to do this unfortunatley. The best workaround would be to create a shortcut file in C:\Program Files\Solid Edge ST9\Template to the location you want, which will at least speed things up a bit.

Re: ST9 - Replace background - default file

Creator
Creator
Go back to your VAR I'm sure they won't mind.

Get them to send you a screen shot of the registry entry.

Post it here too...
Edging since V18

Re: ST9 - Replace background - default file

Gears Phenom Gears Phenom
Gears Phenom

I went back to our VAR  . Smiley Tongue

@adopt-id wrote:

Via Windows -> regedit.exe -> HKEY_LOCAL_MACHINE -> SOFTWARE -> Unigraphics Solutions –> Solid Edge –> Version ST9 à Template path

 

Windows -> regedit.exe -> HKEY_LOCAL_MACHINE -> SOFTWARE -> Wow6432Node ->  Unigraphics Solutions –> Solid Edge –> Version ST9 à Template path

@So, this is a good start, but I also want to choose a default file. @Siemens?
...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: ST9 - Replace background - default file

Creator
Creator

I've never had to do this operation.

 

Could you explain the circumstances of an occasion when you would do this?

 

I usually set up my draft template with all the backgounds I need, using copy and shift-paste to move them from one file to another.

Edging since V18

Re: ST9 - Replace background - default file

Gears Phenom Gears Phenom
Gears Phenom

Our company is moved, so a new address and the logo is changed.

So I made a new background.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: ST9 - Replace background - default file

Creator
Creator

I see, so how many times are you going to do this?

 

If it's a few hundred you might want to get someone to program a macro to do it.

 

I could help you find someone, I only know a bit about programming SE

Edging since V18

Re: ST9 - Replace background - default file

Valued Contributor
Valued Contributor

I just setup a shortcut in the C:\Program Files\Solid Edge ST9\Template folder and this does work to quickly get to to your Template folder. It helps me as my template folder is on another server, so it was several clicks to get to it each time.

 

This needs to be corrected to the default template file in SE options though.

 

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development
Emerson Commercial & Residential Solutions | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA
T +1 419 525 8554

gary.dinges@emerson.com

 

 

Re: ST9 - Replace background - default file

Valued Contributor
Valued Contributor

Is there a reg edit to acomplish this change in ST10 and/or SE 2019?

Posted by Joris above.

 

@adopt-id wrote:

Via Windows -> regedit.exe -> HKEY_LOCAL_MACHINE -> SOFTWARE -> Unigraphics Solutions –> Solid Edge –> Version ST9 à Template path

 

Windows -> regedit.exe -> HKEY_LOCAL_MACHINE -> SOFTWARE -> Wow6432Node ->  Unigraphics Solutions –> Solid Edge –> Version ST9 à Template path

 

I did a search of my registry on Windows 7 Ultimate and did not locate an entry with Templates Path for SE.

 

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Commercial & Residential Solutions | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

Re: ST9 - Replace background - default file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

SE 2019

\HKEY_LOCAL_MACHINE\SOFTWARE\Siemens\Solid Edge\Version 219\TemplatePath

 

SE ST10

\HKEY_LOCAL_MACHINE\SOFTWARE\Unigraphics Solutions\Solid Edge\Version 110\TemplatePath



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com