Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 draft questions.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi~ Currently I'm using ST9, I have some question about  draft fuction.

 

1. When using Draft, when you select dimension, center line, etc.,
Ability to apply colors and layers automatically set in advance.
 
2. When using Draft, replace the color of the hidden line shown in the model's floor plan function.

3. If all of the above functions are available, all colors, layers, etc.
Check if DWG conversion is true
Thanks for in advance.
4 REPLIES

Re: ST9 draft questions.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For 1) change the dimension style to the color you want. Then new dims will show that color. Keep the driven/driving difference in mind. i.e. make them both the same.

For 2 and 3) I don't understand the question.

 

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: ST9 draft questions.

Honored Contributor
Honored Contributor

Layers are not part of perametric modeling & drafting like it is for AutoCAD. No is need for layers, there are other ways to turn things on and off.

Re: ST9 draft questions.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks your reply.

 

First, I'll try your solution~~

Re: ST9 draft questions.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

O.k

Thanks your reply!!!