Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 size of Quick View Cube

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

is it right that the size of the quick view cube in ST9 only can be changed together with the size of coordinate system and the steering wheel in the gloabal options20160727_1028.PNG?

 

I liked it to increase the cube a little bit larger but doing this now brings very ugly steering wheel and CS on the scrren

 

 

regards
Wolfgang
4 REPLIES 4

Re: ST9 size of Quick View Cube

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Yes, that seems odd.

The three together in chorus share the same setting under the Helpers tab.

 

It would have been great if the view cube was sizable from its own settings dialog that already exists.

Re: ST9 size of Quick View Cube

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Agree...it would be nice to control these independently of each other directly in the UI.

I wonder if there is access to such control, via the registry....?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST9 size of Quick View Cube

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Nice hint @SeanCresswell

I spent a few minutes hunting in the deep trenches of the registry, no luck yet.

I too feel sooner or later more users are going to ask for this and development might provide an option in one of the ST 9 MPs itself without waiting for the next release.

Re: ST9 size of Quick View Cube

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


I totally agree with Your comment @Tushar.

Tue to the improvements for high resolution screens this for me seems to be a loss of comfort and ergonomy and it would be very nice if developement could bring back the old (ST8) functionallity with one of the next service packs

 

 

regards
Wolfgang