Cancel
Showing results for 
Search instead for 
Did you mean: 

ST9 to ST10 Student Licence

Creator
Creator

I already have a student licence for ST9 and need to know how to go about updating to ST10?

Is there a place I can go to download ST10 or is it supposed to self update?

7 REPLIES 7

Re: ST9 to ST10 Student Licence

Siemens Phenom Siemens Phenom
Siemens Phenom

You will have to register again, download ST10, uninstall ST9, then install ST10.

https://www.plm.automation.siemens.com/plmapp/education/solid-edge/en_us/free-software/student

 

Re: ST9 to ST10 Student Licence

Creator
Creator

I was able to download but when I try to open it it keeps giving me this message.

 

Required event requires elevation to complete.

 

What does it mean and how do I fix the problem.

 

Any help is greatly appreciated.

 

Thank you.

Re: ST9 to ST10 Student Licence

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Ahweh,

 

Did you complete the steps as @uk_dave said...? [re-stated for clarity below...]

 

  1. Register & download ST10 [latest installation file includes Windows "Fall Creators Update" compatibility]
  2. Uninstall ST9 [right click on Windows app button > Settings > Apps - Solid Edge ST9]
  3. Install ST10 [right click on *.EXE file - select "Run as administrator"]
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: ST9 to ST10 Student Licence

Siemens Phenom Siemens Phenom
Siemens Phenom

"operation requires elevation" is a UAC warning.

 

When you start the ST10 install do not double-click on the exe file to start the install but instead right-click -> Run as Administrator on the exe file to install it.

Re: ST9 to ST10 Student Licence

Creator
Creator
Yes the procedure worked and I am up and running but have a different issue I would like to discuss with someone.

Should I do it in this thread or make another one because it is not related to this at all.

Re: ST9 to ST10 Student Licence

Siemens Phenom Siemens Phenom
Siemens Phenom

Please start a new thread.  TIA

Re: ST9 to ST10 Student Licence

Creator
Creator
Sent from Yahoo Mail on Android