Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

ST9 viewer (view & markup)

Valued Contributor
Valued Contributor

I have a couple of questions.

1. Will the viewer work on 32 bit machines?

2. How/where do you set up the Solid Edge files to be able to be measured by someone with just view/mark-up?

11 REPLIES

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

Viewer is still 32 bit so it will install on either x86 or x64.

 

To set up for measure/markup in Viewer, you need to open the SE file in V&M and save it as a PCF with those options set in the Security/Password options.



Ken

Production: ST10 MP5
Testing: SE 2019

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

Hi @KennyG

 

 

IMHO I have to disagree Your statement.

 

For a couple of version the measurement is available also for non PCF files.

So You directly can open any SE file and You can use the measurment tools in free SE viewer.

 

See picture from SE viewer with an original SE part.20170321_0831.PNG

 

 

 



regards
Wolfgang

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

Hi,

 

 

after sending my last article, I have seen that the question was regarding View&MarkUp and not the free SE viewer.

But the content still is true for the View&MarkUp too.

 

See toolbar for measurement in V&M

You have to decide wether You want to have the measrument from points or edges, for a single eleemnt or for two elements and then select the items, followed by the placement of the dim.

 

20170321_0831.PNG



regards
Wolfgang

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

It's a pretty awful tool for measuring. The interface is awkward and you don't know for sure what you're picking because, unlike in SE, the entities don't highlight until after you pick them.

Bruce Shand
ST10 MP5 - Insight - Win10 - K4200

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

Hi @bshand

 

 

Yes this is absoluteley true!

 

And AFAIK the measurement points might be based on a triangulated boundary,
what also is regarded with the "~" sign in front of the dimension value.

 

But maybe this only is true for a PCF type of document.

 



regards
Wolfgang

Re: ST9 viewer (view & markup)

Valued Contributor
Valued Contributor

I agree that is terrible for measuring.  Is there a better way for non Solid Edge users to take measurements on a DFT file?  We have the Free 2D drafting pkg loaded, but they cannot place dimensions on true SE files.  I have found a workaround - save as a dwg and then re-open the dwg file, but that's sort of a PITA, but it does work.

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

@hawcad You are right!  Missed that change.  Looks like Markups are the only thing still restricted.



Ken

Production: ST10 MP5
Testing: SE 2019

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

Hi @KennyG

 

 

 

... which also sounds in reason since the mark up must be saved somehow and this will be the PCF file

 

- the Package Collaboration File -

 

 



regards
Wolfgang

Re: ST9 viewer (view & markup)

Esteemed Contributor
Esteemed Contributor

@MikeSaari, 3D pdfs are great in this regard as far as models go. Good measure interface.

Bruce Shand
ST10 MP5 - Insight - Win10 - K4200