Cancel
Showing results for 
Search instead for 
Did you mean: 

STD Parts Characteristics not working for this Category

Valued Contributor
Valued Contributor

Hi All,

 

Happy 2016 to you all, havent been on for a while.

 

I have sent this through my reseller and looked on the solution centre and cant see anything

 

The screenshot should clearly show the problem, the i am not getting the thread diameter the the STD parts tool although it is clearly in the administrator. 

 

Any Idea? 

Consultant - Design Majenta PLM - ST10/MP03
3 REPLIES

Re: STD Parts Characteristics not working for this Category

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure what I'm seeing. In the administrator you are showning studs. In the lower standard parts window a nut is showing but it's not clear what is selected. Why would a nut have thread length?

In my standard parts tool a nut the thread diameter is in the thread value column. Like 1/2-13 UNC.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: STD Parts Characteristics not working for this Category

Valued Contributor
Valued Contributor

The problem is that three Characteristics are in the Administrator but only two show up in the STD parts selection tool. In the UN8 section it works correct with the same setup. 

 

 

(nut length is set to 0 btw)

Consultant - Design Majenta PLM - ST10/MP03

Re: STD Parts Characteristics not working for this Category

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I only have one characteristic showing with nuts.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200