Cancel
Showing results for 
Search instead for 
Did you mean: 

STEP & surfaces

Valued Contributor
Valued Contributor

Hello,

 

Sometimes we get a STEP file from a client.

We want to add it as a part into our library for future use, but when we open it in Solid Edge, we get all surfaces (purple, shell), and no solid part. How can we transform a STEP file into a part with mass, no shell only?

 

Thx, Johan

4 REPLIES

Re: STEP & surfaces

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

It depends on many things. It should be "closed" geometry... You can use sew command...

 

Could you post an example?

 

This video can be useful for you:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: STEP & surfaces

Phenom
Phenom

Even though I can't understand the language that presentation demonstrated a lot of great tools. Thank you for sharing.

Re: STEP & surfaces

Phenom
Phenom

If you are getting just surfaces, then you probably have gaps and the translator can not fill the gaps. There are a lot of tools to interogate and fix the geometry.

 

If you can, check to see if you can get a parasolid instead of STEP file. That would provide you with a direct read instead of a translation.

Re: STEP & surfaces

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Sorry for it, hungarian. Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/